Getting a "Card not supported" error when using MicroSD with MK22FN1M0VLL12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting a "Card not supported" error when using MicroSD with MK22FN1M0VLL12

2,750件の閲覧回数
tmd1426
Contributor I

Hey there,

I am getting the kStatus_SDMMC_CardNotSupport error when trying to initialize a microSD card on the board we have built that is using the MK22FN1M0VLL12 MCU.

I'll paste the relevant code below so hopefully someone can assist with the issue:

Screenshot - 041018 - 12_18_32.png

The SD_Init function is where it fails.

Untitled.png

SD_SendApplicationCmd is then where it fails next.

Screenshot - 041018 - 12_27_19.png

Finally, it returns at the if statement there returning kStatus_SDMMC_CardNotSupport.

Can anyone provide any solutions? Thank you for your time.

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,558件の閲覧回数
tmd1426
Contributor I

Hello again,

It's been awhile and I'd like to check and see if there are any other responses from NXP.

0 件の賞賛
返信

2,558件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Thanh Dang 

Before you tried with your own board, did you manage to run the example code in our evaluation board? TWR-K21? this should help to discards any hardware problem. Also, what SD memory are you using? this issue only happened with this memory or have you tried different kinds of memories?

The Card not support status could happen when your clocks are not correct and the card doesn't respond as it should.

Best regards

Jorge Alcala

0 件の賞賛
返信

2,558件の閲覧回数
tmd1426
Contributor I

Hi Jorge,

Thank you. We tried the code on the tower board and received the same error. We are using a MicroSD which we have used with our eval code and it worked successfully. The problem comes when trying to port that eval code over to our production board which is what was posted above.

We have checked the clocks, we are running the bus clock at 374491.

It appears we are getting all zeros back for an R1 response above.

0 件の賞賛
返信