GUI development tool for Kinetis MUC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GUI development tool for Kinetis MUC

1,878 Views
nelsonlobo
Contributor II

Hi,

Was looking for solutions on GUI development using 4.3" TFT screen 40pin parallel connection. Found eGUI available on Freescale website.

Im planning to use the MK02FN64VLH10  MCU. Would the libraries support this MUC. If not then is there any RAD tool for developing screens and buttons using the same ???

Regards,

Nelson Lobo

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

1,540 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Nelson,

Kinetis MCU is supported by the Freescale eGUI and you can find more information through the link as below.

Freescale eGUI: Graphical LCD Driver for MCUs|Freescale
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,540 Views
LuisCasado
NXP Employee
NXP Employee
0 Kudos
Reply