Creating dll in MCU bareboard project with KL26

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Creating dll in MCU bareboard project with KL26

1,547 Views
yusupkhan
Contributor II

Hi,

    i've done a MCU bareboard project with codewarrior for thermal printer  that runs on a KL26.

My project is diveded in a main.c and several .h and .c.; Now I'd like to create a .dll  or a library to hide some .c of my project.

Is there anybody who may give me some hints?

Yusup Khan

0 Kudos
Reply
1 Reply

1,435 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Yusup Khan,

what SW do you work with?

here is article of Creating a Library with Kinetis Design Studio

Creating a Library with Kinetis Design Studio | MCU on Eclipse

if using CW10.6, user can create a customized library with wizard:

2015-10-19_15-19-15.jpg

can this help you?

Zhang Jun 

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply