GUI development tool for Kinetis MUC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GUI development tool for Kinetis MUC

1,932 次查看
nelsonlobo
Contributor II

Hi,

Was looking for solutions on GUI development using 4.3" TFT screen 40pin parallel connection. Found eGUI available on Freescale website.

Im planning to use the MK02FN64VLH10  MCU. Would the libraries support this MUC. If not then is there any RAD tool for developing screens and buttons using the same ???

Regards,

Nelson Lobo

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,594 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Nelson,

Kinetis MCU is supported by the Freescale eGUI and you can find more information through the link as below.

Freescale eGUI: Graphical LCD Driver for MCUs|Freescale
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,594 次查看
LuisCasado
NXP Employee
NXP Employee
0 项奖励
回复