FreescaleCupShieldHelp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreescaleCupShieldHelp

2,285件の閲覧回数
tim_amish
Contributor II

Hi, I was wondering if and how to brake the freescale cup car. Is there some sort of "eddy current brake" or "short brake" capabilities? If so, what code do I need to use to brake the car. I have gone over the tutorial for the freecale cup car and there is nothing about braking (https://community.freescale.com/docs/DOC-93914#jive_content_id_Code_Examples ). Any help would be greatly appreciated.

Cheers,

     Tim

0 件の賞賛
返信
2 返答(返信)

1,983件の閲覧回数
gerhardfreudent
Contributor I

Hi guys,


I am wondering if one ever thought the pinning of the TFC-Shield can be a bit inconvenient. When you wanna add some other sensors, then the camera clock blocks the UART1/I2C1 and the hall sensors block the UART0. So for example when you wanna add the gyro and magnetometer of the BRKT-STBC-AGM01 the you have a problem. Moreover, if you wanna work with Simulink then UART0 is used by the external mode.


So I was wandering if anybody has the same issue and if there will be a new version of the TFC-Shield available or if anyone is interested to design an updated version. We would be very interested to add a gyro and magnetometer as well, since we design an IMU for the car. I have attached a pic which provides information about our desired pinning.


BR,

Gehard

PS:

Pinning_TFC_Shield.png

0 件の賞賛
返信

1,983件の閲覧回数
Stano
NXP Employee
NXP Employee

Hi Tim,

the simplest way to brake the DC brushed motor is to load them by driver (full-bridge MC33887). Simply short circuit two DC motor lines by switch on both bottom full-bridge power MOSFETs. Simply set both outputs to zero.

I think it will help you.

Best Regards,

Stano.

0 件の賞賛
返信