Free SWD programming tool...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Free SWD programming tool...

跳至解决方案
3,072 次查看
rothkarl
Contributor III

Hello Everyone!

I'd like to know if there are any free programming tool exists for Freedom board, something like that ST's ST-Link?

With ST-Link I can burn down any binaries, and erase random sectors I want.

I'am looking for something standalone solution without using Eclipse based IDE.

Thank you!

标签 (1)
0 项奖励
回复
1 解答
2,323 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Roth,

The Freedom board is design to feature the Freescale open standard embedded serial and debug adapter known as OpenSDA.

This circuit offers several options for serial communications, flash programming and run-control debugging.

And you can learn more information about the OpenSDA through the post as below.

OpenSDA on the Freedom KL25Z Board | MCU on Eclipse


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,324 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Roth,

The Freedom board is design to feature the Freescale open standard embedded serial and debug adapter known as OpenSDA.

This circuit offers several options for serial communications, flash programming and run-control debugging.

And you can learn more information about the OpenSDA through the post as below.

OpenSDA on the Freedom KL25Z Board | MCU on Eclipse


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------