Free SWD programming tool...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Free SWD programming tool...

ソリューションへジャンプ
3,147件の閲覧回数
rothkarl
Contributor III

Hello Everyone!

I'd like to know if there are any free programming tool exists for Freedom board, something like that ST's ST-Link?

With ST-Link I can burn down any binaries, and erase random sectors I want.

I'am looking for something standalone solution without using Eclipse based IDE.

Thank you!

ラベル(1)
0 件の賞賛
返信
1 解決策
2,398件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Roth,

The Freedom board is design to feature the Freescale open standard embedded serial and debug adapter known as OpenSDA.

This circuit offers several options for serial communications, flash programming and run-control debugging.

And you can learn more information about the OpenSDA through the post as below.

OpenSDA on the Freedom KL25Z Board | MCU on Eclipse


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,398件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Roth,

The Freedom board is design to feature the Freescale open standard embedded serial and debug adapter known as OpenSDA.

This circuit offers several options for serial communications, flash programming and run-control debugging.

And you can learn more information about the OpenSDA through the post as below.

OpenSDA on the Freedom KL25Z Board | MCU on Eclipse


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------