Flexbus base address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexbus base address

1,784件の閲覧回数
ankurchauhan
Contributor I

I'm using twr-lcd using flexbus (k70).in my case i have FLEX_DC_ADDRESS    0x60000000 but its not working.

its getting stuck somewhere while writing cmd to this address.I find out this by using break-point.

what could be the reason behind this ??

I also tried other address like 0xA0000000 and 0xC0000000.but still result is same.

Regards

Ankur

0 件の賞賛
返信
2 返答(返信)

1,559件の閲覧回数
ankurchauhan
Contributor I

I changed the FLEX_DC_ADDRESS    to 0x80000000, after this change its not getting stuck but still nothing is coming on screen.

what could be the issue.

Regards

Ankur

0 件の賞賛
返信

1,559件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hello Ankur,

please take a look on the Flexbus examples I attached to this post FlexBus in 16 bit mode and 8 bit access

They are usingK60 and K70 with CW and KDS. Some of the examples use TWR.LCD. They ahve also a document explaining the examples.

Regards,

Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信