Flexbus base address

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flexbus base address

1,803 次查看
ankurchauhan
Contributor I

I'm using twr-lcd using flexbus (k70).in my case i have FLEX_DC_ADDRESS    0x60000000 but its not working.

its getting stuck somewhere while writing cmd to this address.I find out this by using break-point.

what could be the reason behind this ??

I also tried other address like 0xA0000000 and 0xC0000000.but still result is same.

Regards

Ankur

0 项奖励
回复
2 回复数

1,578 次查看
ankurchauhan
Contributor I

I changed the FLEX_DC_ADDRESS    to 0x80000000, after this change its not getting stuck but still nothing is coming on screen.

what could be the issue.

Regards

Ankur

0 项奖励
回复

1,578 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hello Ankur,

please take a look on the Flexbus examples I attached to this post FlexBus in 16 bit mode and 8 bit access

They are usingK60 and K70 with CW and KDS. Some of the examples use TWR.LCD. They ahve also a document explaining the examples.

Regards,

Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复