Flexbus SRAM SIZE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexbus SRAM SIZE

2,020 Views
CCandido
Contributor V

Hi,

my teste Flexbus + SRAM  (  IS62WV10248DALL ) 1MBx8

CPU = K22FX512 , Clock = 120, core,bus,flexbus =60

Problems:  0x0000 0000 to 0x0000 7FFF                   ( READ AND WRITE ) = OK

> 0x0000 7FFF , not ( read and write )  ,   return to 0x00000000 page0.

Connection hw:

K22_IS62.bmp

void setup_fb_sram_ (void){

#define SRAM_START_ADDRESS (*(volatile uint32_t*)(0x60000000))

   FB_CSAR0 = (uint32_t)&SRAM_START_ADDRESS;  

   FB_CSCR0 = FB_CSCR_PS(1) // 8-bit port

                        | FB_CSCR_AA_MASK // auto-acknowledge

                                             // | FB_CSCR_ASET(0x1)  // add   assert chip select on second clock edge after address is asserted

                        | FB_CSCR_WS(0x2);                         // 2 wait states

   FB_CSMR0 = FB_CSMR_BAM(0x00FF)                     // 1MB

                        | FB_CSMR_V_MASK                       //Enable cs valid signal

   SIM_SCGC5 |= SIM_SCGC5_PORTB_MASK;           // Enable Clock to PORTB

   SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK;           // Enable Clock to PORTC

   SIM_SCGC5 |= SIM_SCGC5_PORTD_MASK;           // Enable Clock to PORTD

PORTB_PCR11 = PORT_PCR_MUX(5); // fb_ad[18]

  PORTB_PCR16 = PORT_PCR_MUX(5); // fb_ad[17]

  PORTB_PCR17 = PORT_PCR_MUX(5); // fb_ad[16]

  PORTB_PCR18 = PORT_PCR_MUX(5); // fb_ad[15]

  PORTC_PCR0 = PORT_PCR_MUX(5); // fb_ad[14]

  PORTC_PCR1 = PORT_PCR_MUX(5); // fb_ad[13]

  PORTC_PCR2 = PORT_PCR_MUX(5); // fb_ad[12]

  PORTC_PCR4 = PORT_PCR_MUX(5); // fb_ad[11]

  PORTC_PCR5 = PORT_PCR_MUX(5); // fb_ad[10]

  PORTC_PCR6 = PORT_PCR_MUX(5); // fb_ad[9]

  PORTC_PCR7 = PORT_PCR_MUX(5); // fb_ad[8]

  PORTC_PCR8 = PORT_PCR_MUX(5); // fb_ad[7]

  PORTC_PCR9 = PORT_PCR_MUX(5); // fb_ad[6]

  PORTC_PCR10 = PORT_PCR_MUX(5); // fb_ad[5]

  PORTD_PCR2 = PORT_PCR_MUX(5); // fb_ad[4]

  PORTD_PCR3 = PORT_PCR_MUX(5); // fb_ad[3]

  PORTD_PCR4 = PORT_PCR_MUX(5); // fb_ad[2]

  PORTD_PCR5 = PORT_PCR_MUX(5); // fb_ad[1]

  PORTD_PCR6 = PORT_PCR_MUX(5); // fb_ad[0]

  PORTB_PCR20 = PORT_PCR_MUX(5); // fb_ad[31] used as d[7]

  PORTB_PCR21 = PORT_PCR_MUX(5); // fb_ad[30] used as d[6]

  PORTB_PCR22 = PORT_PCR_MUX(5); // fb_ad[29] used as d[5]

  PORTB_PCR23 = PORT_PCR_MUX(5); // fb_ad[28] used as d[4]

  PORTC_PCR12 = PORT_PCR_MUX(5); // fb_ad[27] used as d[3]

  PORTC_PCR13 = PORT_PCR_MUX(5); // fb_ad[26] used as d[2]

  PORTC_PCR14 = PORT_PCR_MUX(5); // fb_ad[25] used as d[1]

  PORTC_PCR15 = PORT_PCR_MUX(5); // fb_ad[24] used as d[0]

  PORTB_PCR19 = PORT_PCR_MUX(5); // fb_oe_b

  PORTC_PCR11 = PORT_PCR_MUX(5); // fb_rw_b

  PORTD_PCR1  = PORT_PCR_MUX(5); // fb_cs0_b

  }

//---------------------------------------SRAM WRITE

void sram_write_byte ( uint32_t adress , byte valor ){

*(volatile uint32_t*)( &SRAM_START_ADDRESS +  adress ) = valor;

}

//---------------------------------------SRAM READ

byte sram_read_byte(uint32_t adress ){

return( *(volatile uint32_t*)( &SRAM_START_ADDRESS +  adress  ));

}

//------------------------------------

thanks;

Carlos.

Labels (1)
0 Kudos
Reply
3 Replies

1,723 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Carlos,

can you share your whole Flexbus configuration?

Regards,

Carlos

0 Kudos
Reply

1,723 Views
CCandido
Contributor V

Hi Carlos,

The complete configuration is the same, alas this whole code.

I can read and write (0x0000 to 0x7FFF),

higher addresses can not be reached, eventually returning to BASE_SRAM.

one thing I noticed,arises proper value in  FB_CSMR_BAM (0x000F (1MB)  ) = ERROR FLEXBUSS. not init cpu.

thanks,

Carlos.

0 Kudos
Reply

1,723 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Carlos,

You must use FB_CSMR0 = FB_CSMR_BAM(0xF);

Please check if the register value is set correctly. Otherwise check hardware connection, most likely this is the problem.

Regards,

Carlos

0 Kudos
Reply