FlexNVM/FlexRAM Example? (AN4282)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FlexNVM/FlexRAM Example? (AN4282)

跳至解决方案
3,484 次查看
lsrbigfoot
Contributor IV

I am looking to implement AN4282 (Enhanced EEPROM Functionality) on a Kinetis K22 micro using the KSDK drivers (fsl_flash.h & fsl_flash.c). Are there any AN4282 related code examples available? Where can I find them?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
3,096 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Customer could visit MCUXpresso SDK to build&download SDK package for [FRDM-KE15Z] board.

There provides [flexnvm_eeprom] demo for customer reference with below path:

..\FRDM-KE15Z\boards\frdmke15z\driver_examples\flash\flexnvm_eeprom

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
3,097 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Customer could visit MCUXpresso SDK to build&download SDK package for [FRDM-KE15Z] board.

There provides [flexnvm_eeprom] demo for customer reference with below path:

..\FRDM-KE15Z\boards\frdmke15z\driver_examples\flash\flexnvm_eeprom

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,096 次查看
lsrbigfoot
Contributor IV

Thanks! This helped. The frdmke15z driver files (fsl_flash and other pieces [like fsl_ftfx_controller and fsl_ftfx_nvmem]) appear to be a different implementation when compared with MK22F512A's driver files (large fsl_flash driver).

How compatible are frdmke15z's_flash related driver files with the current MK22F512A and its fsl_features?

0 项奖励
回复
3,096 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

KE15 FlexNVM working as EEPROM flash commands is same with MK22FX512A.

Customer could refer and using related driver for MK22FX512A.

The only difference is the FlexNVM and FlexRAM memory size:

KE15:

FlexNVM = 32KB & FlexRAM = 2KB  sector size is 2KB;

MK22FX512A:

FlexNVM = 128KB & FlexRAM = 4KB  sector size is 4KB;

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复