Field programming using some utility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Field programming using some utility

ソリューションへジャンプ
2,847件の閲覧回数
sudhanshumehta
Contributor IV

Hello Everyone,

 

We use P&E micro multilink universal FX debugger/programmers for NXP kinetis microcontroller. 

If we want to update firmware in field, is there is any utility which we can give to our field technicians to reprogram updated firmware? We are using K22 and K70 controllers.

Currently I see option in KDS IDE etc. but I am looking for some easy utility for field technicians.. any help will be great..

 

Thanks

Sudhanshu

0 件の賞賛
返信
1 解決策
2,841件の閲覧回数
dacapn
Contributor I

I never used this but there is an official tool from the debugger manufacturer:

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320181&productTab=1

also, there is a similar thread where you can get more info:

https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-tool-SWD-JTAG/m-p/1183765/highlight/fals...

Worst case scenario, your technicians will have to learn programming from the IDE which isn't a deal breaker if they can use the other tools.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,842件の閲覧回数
dacapn
Contributor I

I never used this but there is an official tool from the debugger manufacturer:

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320181&productTab=1

also, there is a similar thread where you can get more info:

https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-tool-SWD-JTAG/m-p/1183765/highlight/fals...

Worst case scenario, your technicians will have to learn programming from the IDE which isn't a deal breaker if they can use the other tools.

0 件の賞賛
返信
2,356件の閲覧回数
sukyeong
Contributor III

Hello, @dacapn 

I am looking for a tool that can easily update the firmware as above.

 

I use P&E micro multilink universal debugger/programmers for NXP

i'm using i.MXRT1176 chip

Currently I see option in MCUXPressoIDE . 

 

I tried using the PROGDSC(Flash Programmer) tool, but it doesn't seem to work, so I am inquiring

 

Thanks

タグ(1)
0 件の賞賛
返信