FTM2 CH0 to generate simple clock of 16khz

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FTM2 CH0 to generate simple clock of 16khz

2,046 次查看
Rashmitha_Nair
Contributor III

Hi,

I am trying to generate a simple clock of 16khz using a FTM2 CH0 and below is my initialization code

void startClock() //FTM2 CH0 16khz
{
	/**********************************************************************************
	 * PORT SETUP
	 * ********************************************************************************
	 */

	// System Clock Gating Control Register 5 (SIM_SCGC5), switch on clock for port B
	*(volatile unsigned long *)(SIM_BLOCK + SIM_PORT_CLK_GATE_OFFSET) |= 0x400;

    // FTM2_CH0 on PTB18 (alt. function 3) and high drive strength
    *(volatile unsigned long *)(PORTB_BLOCK + 0x48) |= (0x00000300 | 0x00000040);

 	/**********************************************************************************
 	 * Flex Timer 2 Channel 0 Setup
 	 * ********************************************************************************
 	 */

 	// FTM2. Ensure that the FlexTimer/TPM module is powered up
     *(volatile unsigned long *)(SIM_BLOCK + 0x103c) |= 0x4000000;

    // FTM Status And Control (FTM0_SC). Disable FTM2 operation (system clock)
    *(volatile unsigned long *)(FTM2_BASE_ADDR + 0x000) = 0x00000000;

    // Configuration (FTMx_CONF) pp 1020
    // pin
    // 6 - 7 - BDM mode 3 - 0xc0 (allow timer to continue operating when debugging)
    // 9     - Enable use of global timebase from another FTM module 0x200 (Unused here)
    // 10 	 - Enable output of global timebase to other FTMs 0x400 (unused here)
    *(unsigned long *)(FTM2_BASE_ADDR + 0x084) = (0x000000c0);

    // Disable Write protection on the FTMx_MODE.
    *(unsigned long *)(FTM2_BASE_ADDR + 0x054) = 0x00000004;

    // Features Mode Selection (FTMx_MODE)
    // Switch off the enhanced FTM features to avoid needing to do an explicit software load of the CnV regs.
    // Keep write protection disabled - 0x04
    *(unsigned long *)(FTM2_BASE_ADDR + 0x054) = (0x00000004 | 0x0000000);

    // Synchronisation (FTMx_SYNC).
    // Enable loading at maximum (i.e. CV == MOD) - 0x00000002
    // Software triggering is enabled - 0x80
    *(unsigned long *)(FTM2_BASE_ADDR + 0x58) = (0x00000002 | 0x80);

    // Set counter MOD register to the value that provides the frequency of interest.
    // 0x3C6  - 1 kHz with a pre-scaler of 128
    // 0x0BB; - 320 kHz
    *(unsigned long *)(FTM2_BASE_ADDR + FTM2_MOD) =  3750-1;//0x0BB;// - 320 kHz;

    // Synchronisation Configuration (FTMx_SYNCONF)
    // set SYNCMODE (Enhanced PWM synchronisation is selected.) - 0x80
    // set SWRSTCNT = 1 (FTM counter synchronisation is activated by the software trigger) - 0x100
    // set SWWRBUF = 1 (MOD, CNTIN, and CV registers synchronisation is activated by the software trigger.) - 0x200
    *(unsigned long *)(FTM2_BASE_ADDR + 0x8C) = (0x200);

    // Channel (n) Status And Control (FTMx_CnSC)
    // ELSnB:ELSnA = 1:0 Edge-Aligned PWM High-true pulses (clear Output on match) - 0x08
    // MSnB:MSnA = 1:0 (See ELSnB:ELSnA) - 0x20
    *(volatile unsigned long *)(FTM2_BASE_ADDR + FTM2_C0SC_OFFSET) = (0x00000020 | 0x00000008);

    // Set counter initial value to zero
    *(volatile unsigned long *)(FTM2_BASE_ADDR + 0x04c) = 0;
    *(volatile unsigned long *)(FTM2_BASE_ADDR + 0x060) = 0x01;
    // prepare first PWM value (place it in the CnV register)
    *(volatile unsigned long *)(FTM2_BASE_ADDR + FTM2_C0V_OFFSET) = 3750/2;//0x5D;//0x1E3;
}

 

I am generating an SPWM on FTM0 CH6 and 7 too, so I am enabling both the FTM modules together after initializing the FTM0 module as below.

 

     /**********************************************************************************
   * Enable Clock to FTM module.
   * ********************************************************************************
   */

     // FTM Status And Control (FTM0_SC). Enable FTM0 operation (system clock)
     *(volatile unsigned long *)(FTM0_BASE_ADDR + 0x000) = 0x00000008;
    // FTM Status And Control (FTM2_SC). Enable FTM2 operation (system clock)
     *(volatile unsigned long *)(FTM2_BASE_ADDR + 0x000) = 0x00000008;

 

I am getting the SPWM output on PTA 1/2 but the FTM2 clock output on PTB18 isn't getting generated. The output is turned ON and OFF using GPIOB Pin 19.

Is there some settings that are missing in the above code? I have enabled the clock to PORTB & PORTA in board init.

 

Regards,

Rashmitha

0 项奖励
回复
2 回复数

2,012 次查看
troelsoesteraa
Contributor III

Hi,

Did you get this to work?

If you weren't aware, NXP supplies header files for each of the Kinetis processor series, so you don't need to hard-code the base offsets.

I don't see an immediate problem in your code, but I would leave out everything regarding synchronization, when all you want to do is to generate a PWM at 16 kHz and 50% duty cycle.

I would also re-arrange the order a bit, so that the channel specific stuff is the first thing that is defined. Otherwise, the following is pretty much how you already configure the FTM2.

// Set FTM mode to edge-aligned PWM, clear output on match.
FTM2->CONTROLS[0].CnSC = FTM_CnSC_MSB_MASK | FTM_CnSC_ELSB_MASK;
FTM2->CONTROLS[0].CnV = 3750/2;
   
// Ensure that write protection of FTM_SC_REG is off (it always should be).
FTM2->MODE |= FTM_MODE_WPDIS_MASK;
// Make sure we are using legacy (non-FTM) behavior. This should be default,
// but is important to meet buffered updates of FTM_CnV_REG, as mentioned in Sec. 38.4.10.3. (MK22FN256VLL12 user manual)
FTM2->MODE &= ~FTM_MODE_FTMEN_MASK;
// Make sure that FTM (PWM) is running in JTAG/debug modes as well.
FTM2->CONF = FTM_CONF_BDMMODE(3);    
// Load MOD (modulus) or overflow value. This is the PWM freq which applies across the whole FTM2 module.
FTM2->MOD = 3750;
// Reset counter value    
FTM2->CNT = 0;
// Reset initial counter value. This is also reset by selecting a clock source in FTM_SC_CLKS.
// Must always be 0 for EPWM (Sec. 38.4.6)
FTM2->CNTIN = 0;
// Enable FTM with bus clock with no prescaler.    
FTM2->SC = FTM_SC_CLKS(1) | FTM_SC_PS(0);


Hope this helps.

Kind regards,
Troels

 

0 项奖励
回复

2,031 次查看
Ramon_Vega
NXP TechSupport
NXP TechSupport

 

Dear Rashmitha,

Thank you so much for your patience, please check this information below, I hope it be useful:

I truly recommend  download and install MCUXpresso IDE,

Once installed you can import examples about FTM in your IDE to debug and run it on your development board.

Download the following SDK:  Dashboard | MCUXpresso SDK Builder (nxp.com)

  • To install drag and drop the file in MCUXpresso installed SDKs section, please see the picture.

Ramon_delaVega_0-1656628428008.png

 

  • Create new project, please press this option.

 Ramon_delaVega_1-1656628428018.png

  • Select the correct board then press next.

Ramon_delaVega_2-1656628428193.png

  • You will be able to find different kind of examples about FTM.

Ramon_delaVega_3-1656628428240.png

When you get at this point, you can enable FTM2 with your clock preferences, just follow the next steps:

  1. Please click in peripherals, it is right top in screen:

Ramon_delaVega_4-1656628428272.png

 

 

  1. Enable peripherals as in the picture if its needed then close.

Ramon_delaVega_5-1656628428300.png

 

  1. Left side please select the FTM you want to enable and choose clock frecuency, then press Update Code button, this will generate code to enable the FTM as you want.

Ramon_delaVega_6-1656628428395.png

 

Last step is consult the generated code in the following files then you can use them in the main file called “ftm_pwm_twochannel.c”.

Ramon_delaVega_7-1656628531567.png

I hope this information be useful, please let me know for any other question.

 

Best Regards.

-Ramon.

                                                       

0 项奖励
回复