FRDM-K66 Mechanical / 3D Model / BRD File

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-K66 Mechanical / 3D Model / BRD File

2,562 次查看
philipp_zh
Contributor II

Hi,

I am looking into making a shield for the K66 and was wondering if anybody has a mechanical drawing or even 3D model of the board. Other boards' design files include the Allegro .brd file, from which an accurate mechanical model could be derived, too.

For just the pin headers, I am aware that the mechanicals are the same as for the Arduino R3.

Thanks,
Philipp

标记 (1)
2 回复数

2,226 次查看
miduo
NXP Employee
NXP Employee

Hi,

You can download the board design file from the link below:

http://www.nxp.com/assets/downloads/data/en/printed-circuit-boards/FRDM-K66F-DF.zip 

0 项奖励
回复

2,226 次查看
whata
Contributor III

Li,

The files that you're referring to do not contain the actual pcb file, Allegro tool from Cadence store their board files with extension .brd, while the files in the allegro\ directory are of type .dat  Can you also attach the dxf/dwg output of the board, because Cadence Allegro viewer does not support export function.

0 项奖励
回复