External RAM on KL25Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

External RAM on KL25Z

2,081 次查看
jairo15
Contributor I

Hello,

I need help to interface an external RAM in KL25Z.

I need to build a buffer with 64kB.

Can anyone help me?

Thanks.

3 回复数

1,800 次查看
Monica
Senior Contributor III

Hello Jairo,

How is the project going, did this solved your questions?

Please let us know :smileywink:

Regards,

Monica

0 项奖励
回复

1,800 次查看
jairo15
Contributor I

Hi Monica,

My project is summarized in a speech delay, with the internal memory has managed to make it work for 1 sec.

I need more time, nearly 5 seconds I think to use RAM SPI 23LC1024 to do this, but I have not found in the local market, so I can report the results.

1,800 次查看
Paul_Tian
NXP Employee
NXP Employee

As you know, KL series product has not Flex bus, so it is not suitable to do your application. We recommend Kinetis K series product for you. If you have to use KL25, I think it depends on which function you need. If you need to store data temporary, I think you can use GPIO to simulate. If code, KL25 cannot use in this way.