External RAM on KL25Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External RAM on KL25Z

2,183件の閲覧回数
jairo15
Contributor I

Hello,

I need help to interface an external RAM in KL25Z.

I need to build a buffer with 64kB.

Can anyone help me?

Thanks.

ラベル(2)
3 返答(返信)

1,902件の閲覧回数
Monica
Senior Contributor III

Hello Jairo,

How is the project going, did this solved your questions?

Please let us know :smileywink:

Regards,

Monica

0 件の賞賛
返信

1,902件の閲覧回数
jairo15
Contributor I

Hi Monica,

My project is summarized in a speech delay, with the internal memory has managed to make it work for 1 sec.

I need more time, nearly 5 seconds I think to use RAM SPI 23LC1024 to do this, but I have not found in the local market, so I can report the results.

1,902件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

As you know, KL series product has not Flex bus, so it is not suitable to do your application. We recommend Kinetis K series product for you. If you have to use KL25, I think it depends on which function you need. If you need to store data temporary, I think you can use GPIO to simulate. If code, KL25 cannot use in this way.