Error[Pe1305]: function declared with "noreturn"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error[Pe1305]: function declared with "noreturn"

1,534件の閲覧回数
oscarrazo
Contributor I

Hi all. i just downloaded the FSL_Kinetis_Bootloader_1_1_0 source code, i did not performed any modifications yet, but when compiling i'm getting the next error: Error[Pe1305]: function declared with "noreturn" does retrun. Can you please advice? I am using the IAR Embedded Workbench IDE - ARM 8.11.1 Best Regards

Please see below:

pastedImage_2.png

タグ(1)
0 件の賞賛
返信
1 返信

1,380件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Oscar Razo

This is a IDE related problem, I test the same code in IAR Embedded Workbench IDE - ARM 7.60.1 and it could compile without problems. Regardless of this, my recommendation is that you use the latest version of Kinetis bootloader, which is the version NXP_Kinetis_Bootloader_2.0.0

Best Regards

Jorge Alcala

0 件の賞賛
返信