Dose K60 support quad spi NOR flash mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Dose K60 support quad spi NOR flash mode?

跳至解决方案
1,979 次查看
楊智翔楊
Contributor II

Dose the K60 support quad spi flash mode?If can't,is possible to use sdcard spi bsp driver to do it?How to do?Thanks!

NorFlash is Micron Serial NOR Flash Memory,model is N25Q064A.

0 项奖励
回复
1 解答
1,831 次查看
cutworth
NXP Employee
NXP Employee

No, you cannot use K60 for connecting QuadSPI. QuadSPI requires four data lines while K60 SPI module can just support one data in and one data out like typical SPI interface. 

For connecting QuadSPI, you need to use K80.

Hao

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,832 次查看
cutworth
NXP Employee
NXP Employee

No, you cannot use K60 for connecting QuadSPI. QuadSPI requires four data lines while K60 SPI module can just support one data in and one data out like typical SPI interface. 

For connecting QuadSPI, you need to use K80.

Hao

0 项奖励
回复