Dose K60 support quad spi NOR flash mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dose K60 support quad spi NOR flash mode?

Jump to solution
1,982 Views
楊智翔楊
Contributor II

Dose the K60 support quad spi flash mode?If can't,is possible to use sdcard spi bsp driver to do it?How to do?Thanks!

NorFlash is Micron Serial NOR Flash Memory,model is N25Q064A.

0 Kudos
Reply
1 Solution
1,834 Views
cutworth
NXP Employee
NXP Employee

No, you cannot use K60 for connecting QuadSPI. QuadSPI requires four data lines while K60 SPI module can just support one data in and one data out like typical SPI interface. 

For connecting QuadSPI, you need to use K80.

Hao

View solution in original post

0 Kudos
Reply
1 Reply
1,835 Views
cutworth
NXP Employee
NXP Employee

No, you cannot use K60 for connecting QuadSPI. QuadSPI requires four data lines while K60 SPI module can just support one data in and one data out like typical SPI interface. 

For connecting QuadSPI, you need to use K80.

Hao

0 Kudos
Reply