Does the Kinetis K6X support auto negotiation, auto crossover, dhcp and ntp?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the Kinetis K6X support auto negotiation, auto crossover, dhcp and ntp?

ソリューションへジャンプ
1,667件の閲覧回数
erikk
Contributor I

Hello,

I want to select a microcontroller for my purpose. Thats why I need to know if any of the Kinetis K6X microcontroller supports autonegotiation, auto crossover, dhcp and ntp?

With best regards,
Erik Kliemt

ラベル(1)
0 件の賞賛
返信
1 解決策
1,507件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Erik,

auto-negotiation and auto-crossover are controlled by the Ethernet PHY, so if you select the proper PHY, there will be no problem to use these functions. For K6X MCUs, we provide sdk 2.0 which integrates lwIP 2.0.0 RC0, you may find dhcp and sntp(Simple network time protocol) supports in it. Please kindly refer to Welcome to MCUXpresso | MCUXpresso Config Tools  for details.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,508件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Erik,

auto-negotiation and auto-crossover are controlled by the Ethernet PHY, so if you select the proper PHY, there will be no problem to use these functions. For K6X MCUs, we provide sdk 2.0 which integrates lwIP 2.0.0 RC0, you may find dhcp and sntp(Simple network time protocol) supports in it. Please kindly refer to Welcome to MCUXpresso | MCUXpresso Config Tools  for details.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,507件の閲覧回数
mjbcswitzerland
Specialist V

Hi

It is the Ethernet PHY that performs auto-negotiation and auto-crossover and not the Ethernet controller. If you choose a suitable PHY then you will have these features with any K5x, K6x or K7x part.

DHCP and NPT are software layers and have nothing to do with the Ethernet controller. If you use a suitable TCP/IP stack you will also have these.

Eg.
http://www.utasker.com/docs/uTasker/uTaskerDHCP.pdf
http://www.utasker.com/docs/uTasker/uTaskerSNTP.pdf

Regards

Mark

0 件の賞賛
返信