Does the Kinetis K6X support auto negotiation, auto crossover, dhcp and ntp?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the Kinetis K6X support auto negotiation, auto crossover, dhcp and ntp?

Jump to solution
1,646 Views
erikk
Contributor I

Hello,

I want to select a microcontroller for my purpose. Thats why I need to know if any of the Kinetis K6X microcontroller supports autonegotiation, auto crossover, dhcp and ntp?

With best regards,
Erik Kliemt

Labels (1)
0 Kudos
Reply
1 Solution
1,486 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Erik,

auto-negotiation and auto-crossover are controlled by the Ethernet PHY, so if you select the proper PHY, there will be no problem to use these functions. For K6X MCUs, we provide sdk 2.0 which integrates lwIP 2.0.0 RC0, you may find dhcp and sntp(Simple network time protocol) supports in it. Please kindly refer to Welcome to MCUXpresso | MCUXpresso Config Tools  for details.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,487 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Erik,

auto-negotiation and auto-crossover are controlled by the Ethernet PHY, so if you select the proper PHY, there will be no problem to use these functions. For K6X MCUs, we provide sdk 2.0 which integrates lwIP 2.0.0 RC0, you may find dhcp and sntp(Simple network time protocol) supports in it. Please kindly refer to Welcome to MCUXpresso | MCUXpresso Config Tools  for details.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,486 Views
mjbcswitzerland
Specialist V

Hi

It is the Ethernet PHY that performs auto-negotiation and auto-crossover and not the Ethernet controller. If you choose a suitable PHY then you will have these features with any K5x, K6x or K7x part.

DHCP and NPT are software layers and have nothing to do with the Ethernet controller. If you use a suitable TCP/IP stack you will also have these.

Eg.
http://www.utasker.com/docs/uTasker/uTaskerDHCP.pdf
http://www.utasker.com/docs/uTasker/uTaskerSNTP.pdf

Regards

Mark

0 Kudos
Reply