Does the Kinetis K6X support auto negotiation, auto crossover, dhcp and ntp?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does the Kinetis K6X support auto negotiation, auto crossover, dhcp and ntp?

跳至解决方案
1,658 次查看
erikk
Contributor I

Hello,

I want to select a microcontroller for my purpose. Thats why I need to know if any of the Kinetis K6X microcontroller supports autonegotiation, auto crossover, dhcp and ntp?

With best regards,
Erik Kliemt

标签 (1)
0 项奖励
回复
1 解答
1,498 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Erik,

auto-negotiation and auto-crossover are controlled by the Ethernet PHY, so if you select the proper PHY, there will be no problem to use these functions. For K6X MCUs, we provide sdk 2.0 which integrates lwIP 2.0.0 RC0, you may find dhcp and sntp(Simple network time protocol) supports in it. Please kindly refer to Welcome to MCUXpresso | MCUXpresso Config Tools  for details.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,499 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Erik,

auto-negotiation and auto-crossover are controlled by the Ethernet PHY, so if you select the proper PHY, there will be no problem to use these functions. For K6X MCUs, we provide sdk 2.0 which integrates lwIP 2.0.0 RC0, you may find dhcp and sntp(Simple network time protocol) supports in it. Please kindly refer to Welcome to MCUXpresso | MCUXpresso Config Tools  for details.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,498 次查看
mjbcswitzerland
Specialist V

Hi

It is the Ethernet PHY that performs auto-negotiation and auto-crossover and not the Ethernet controller. If you choose a suitable PHY then you will have these features with any K5x, K6x or K7x part.

DHCP and NPT are software layers and have nothing to do with the Ethernet controller. If you use a suitable TCP/IP stack you will also have these.

Eg.
http://www.utasker.com/docs/uTasker/uTaskerDHCP.pdf
http://www.utasker.com/docs/uTasker/uTaskerSNTP.pdf

Regards

Mark

0 项奖励
回复