Does the KL25 require a crystal to run?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the KL25 require a crystal to run?

ソリューションへジャンプ
1,953件の閲覧回数
l0wside
Contributor II

In a small application, I am considering to replace the existing TI MSP430 with a Kinetis KL25 - twice the memory at half the price is just too tempting.

The current application does not require a crystal, and given the tiny size of my board (and the extra cost), I am not eager to use one. Can the Kienis KL25 (and others from the KL1... and KL2... series) be used with an internal oscillator? If so, what is the tolerance of the oscillator? What is the maximum processor speed with an internal oscillator?

Of course, this is RTFM, but to be honest: the Reference Manual has rather confused than enlightened me.

Max

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,791件の閲覧回数
BlackNight
NXP Employee
NXP Employee

yes, you can run it with the internal reference clock (no external oscillator needed). You need an external crystal on the KL25Z if you want to use USB.

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,792件の閲覧回数
BlackNight
NXP Employee
NXP Employee

yes, you can run it with the internal reference clock (no external oscillator needed). You need an external crystal on the KL25Z if you want to use USB.

Erich

0 件の賞賛
返信