Does the KL25 require a crystal to run?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does the KL25 require a crystal to run?

跳至解决方案
1,956 次查看
l0wside
Contributor II

In a small application, I am considering to replace the existing TI MSP430 with a Kinetis KL25 - twice the memory at half the price is just too tempting.

The current application does not require a crystal, and given the tiny size of my board (and the extra cost), I am not eager to use one. Can the Kienis KL25 (and others from the KL1... and KL2... series) be used with an internal oscillator? If so, what is the tolerance of the oscillator? What is the maximum processor speed with an internal oscillator?

Of course, this is RTFM, but to be honest: the Reference Manual has rather confused than enlightened me.

Max

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,794 次查看
BlackNight
NXP Employee
NXP Employee

yes, you can run it with the internal reference clock (no external oscillator needed). You need an external crystal on the KL25Z if you want to use USB.

Erich

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,795 次查看
BlackNight
NXP Employee
NXP Employee

yes, you can run it with the internal reference clock (no external oscillator needed). You need an external crystal on the KL25Z if you want to use USB.

Erich

0 项奖励
回复