Does anyone know if configuring the FRDM-K64F FTM ( flexible timer module) to use an external clock that if the external clock period can be infinite.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does anyone know if configuring the FRDM-K64F FTM ( flexible timer module) to use an external clock that if the external clock period can be infinite.

1,567 次查看
darringarrett
Contributor I

I need clock the FTM with an external clock that is driven off of a magnetic pickup mounted to a shaft of a motor.  This motor rotates from  equal to 0 rpm to 4000 rpm.

0 项奖励
回复
2 回复数

1,308 次查看
apanecatl
Senior Contributor II

In theory it is infinite, for your specific case I don't think you will face any problem using your clock source (4,000/60=66.66Hz).

0 项奖励
回复

1,308 次查看
darringarrett
Contributor I

Thanks Pedro,  I am mostly concerned about the ability of the clock to function from 0 rpm and up from there.  So if the FTM can be clocked at very low frequencies then I could use this board.

0 项奖励
回复