Does anyone know if configuring the FRDM-K64F FTM ( flexible timer module) to use an external clock that if the external clock period can be infinite.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does anyone know if configuring the FRDM-K64F FTM ( flexible timer module) to use an external clock that if the external clock period can be infinite.

2,132件の閲覧回数
darringarrett
Contributor I

I need clock the FTM with an external clock that is driven off of a magnetic pickup mounted to a shaft of a motor.  This motor rotates from  equal to 0 rpm to 4000 rpm.

0 件の賞賛
返信
2 返答(返信)

1,873件の閲覧回数
apanecatl
Senior Contributor II

In theory it is infinite, for your specific case I don't think you will face any problem using your clock source (4,000/60=66.66Hz).

0 件の賞賛
返信

1,873件の閲覧回数
darringarrett
Contributor I

Thanks Pedro,  I am mostly concerned about the ability of the clock to function from 0 rpm and up from there.  So if the FTM can be clocked at very low frequencies then I could use this board.

0 件の賞賛
返信