Do Freedom boards arrive with Arduino connectors pre-installed or not ? On both sides?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Do Freedom boards arrive with Arduino connectors pre-installed or not ? On both sides?

跳至解决方案
1,038 次查看
Anonymous
不适用

I want to order FRDM-K64F but it is not clear if it comes with connectors already installed. The user manual shows female Arduino sockets on the top layer, not clear whether there are male connectors on the other side. I need connectors on the bottom side to connect this board to my motherboard. Is it possible to order this board without connectors installed? Or are there male connectors on the bottom side by default?

Please let me know.

标记 (2)
0 项奖励
回复
1 解答
947 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

No, FRDM-K64F doesn't have mail Arduino connectors on the bottom side, and yes, the female Arduino sockets on the top layer are pre-installed by default. You have to change the connectors manually. Sorry for the inconvenience that might cause.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
948 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

No, FRDM-K64F doesn't have mail Arduino connectors on the bottom side, and yes, the female Arduino sockets on the top layer are pre-installed by default. You have to change the connectors manually. Sorry for the inconvenience that might cause.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复