Diable GPIO in UART pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Diable GPIO in UART pins

ソリューションへジャンプ
2,199件の閲覧回数
boominperera
Contributor I

Hi,

Does anyone know how I could disable the UART0 in pins (PTB1 and PTB2). I need to disable the UART0 entirely to go into LLS mode so that is very little current consumption.This is in the Frdm KL05Z board.

Thanks

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,126件の閲覧回数
mjbcswitzerland
Specialist V

Hi Boomin

If you add an internal pull-up to the UART Rx it should give you lowest power consumption (to avoid floating). Driving an output in LLS mode should not be an issue.

Regards

Mark


Kinetis: http://www.utasker.com/kinetis.html

KL05
- http://www.utasker.com/kinetis/FRDM-KL05Z.html (with LLS mode reference)
- LLS Video on FRDM-KL05Z https://www.youtube.com/watch?v=iZEMRiDmHzw&feature=youtu.be

元の投稿で解決策を見る

2 返答(返信)
2,126件の閲覧回数
boominperera
Contributor I

Hi Mark,

It works, Thank you

0 件の賞賛
返信
2,127件の閲覧回数
mjbcswitzerland
Specialist V

Hi Boomin

If you add an internal pull-up to the UART Rx it should give you lowest power consumption (to avoid floating). Driving an output in LLS mode should not be an issue.

Regards

Mark


Kinetis: http://www.utasker.com/kinetis.html

KL05
- http://www.utasker.com/kinetis/FRDM-KL05Z.html (with LLS mode reference)
- LLS Video on FRDM-KL05Z https://www.youtube.com/watch?v=iZEMRiDmHzw&feature=youtu.be