Device is Secure. Erase ........

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Device is Secure. Erase ........

Jump to solution
2,061 Views
JHinkle
Senior Contributor I

I have a K60 tower board.

CW 10.4 --- just downloaded.

Created a bare bone project using GNU compiler.

Compiled project --- all well.

P&E interface to load and debug.

Get .... Device is secure.  Erase to unsecure?  YES ....

System halts ....   Memory dump of address zero shows all vectors are erased but the simple bare bone program was not flashed,.

What needs to be done to unsecure the device since it appears P&E is not able to do it on its own.

Any help --- thanks in advance.

Joe

1 Solution
1,768 Views
JHinkle
Senior Contributor I

Fixed it ....

The twr board has a K60F.

My application --- I am writing a bootloader for a K60D

Remade app for K60F --- all is well.

Joe

View solution in original post

2 Replies
1,769 Views
JHinkle
Senior Contributor I

Fixed it ....

The twr board has a K60F.

My application --- I am writing a bootloader for a K60D

Remade app for K60F --- all is well.

Joe

1,768 Views
Monica
Senior Contributor III

Joe,

great to know! Thanks a lot for sharing! :smileygrin:

Best regards,

Monica

0 Kudos
Reply