Device is Secure. Erase ........

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device is Secure. Erase ........

ソリューションへジャンプ
2,131件の閲覧回数
JHinkle
Senior Contributor I

I have a K60 tower board.

CW 10.4 --- just downloaded.

Created a bare bone project using GNU compiler.

Compiled project --- all well.

P&E interface to load and debug.

Get .... Device is secure.  Erase to unsecure?  YES ....

System halts ....   Memory dump of address zero shows all vectors are erased but the simple bare bone program was not flashed,.

What needs to be done to unsecure the device since it appears P&E is not able to do it on its own.

Any help --- thanks in advance.

Joe

1 解決策
1,838件の閲覧回数
JHinkle
Senior Contributor I

Fixed it ....

The twr board has a K60F.

My application --- I am writing a bootloader for a K60D

Remade app for K60F --- all is well.

Joe

元の投稿で解決策を見る

2 返答(返信)
1,838件の閲覧回数
JHinkle
Senior Contributor I

Fixed it ....

The twr board has a K60F.

My application --- I am writing a bootloader for a K60D

Remade app for K60F --- all is well.

Joe

1,838件の閲覧回数
Monica
Senior Contributor III

Joe,

great to know! Thanks a lot for sharing! :smileygrin:

Best regards,

Monica

0 件の賞賛
返信