Development board FRDM-K64F and embed enablement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Development board FRDM-K64F and embed enablement

ソリューションへジャンプ
3,844件の閲覧回数
neilporven
Senior Contributor I

Hi everyone,

I am testing with the development board FRDM-K64F.  I am using embed enablement and find it great to work with, but

now I am afraid that I can't port the library to the Kinetis Design Studio.  Has anyone used embed enablement and ported

their test code to the Kinetis Design Studio?  If you have, how is this done? Is there documentation?

Thank you,

Neil Porven

ラベル(2)
1 解決策
3,679件の閲覧回数
santiago_lopez
NXP Employee
NXP Employee

Hi Neil,

These are the steps I followed in order to migrate my project.

1. Right click on the mbed project and select Export Program

Step_1.png

2. Click on the drop-down list and select Kinetis Design Studio. Then click on Export

Step_2.png

3. A ZIP file will be downloaded. Extract this file to a known location.

Step_3.png

4. Open Kinetis Design Studio. On the Project Explorer region, right click and select import.

Step_4.png

5. Select Existing Projects into Workspace and click Next

Step_5.png

6. Click on Browse and select the location of the uncompressed folder

Step_6.png

7. Make sure that your project is checked and click on Finish

Step_7.png

After this your project should apear in the Project Explorer

Step_8.png

Saludos

Santiago Lopez -- Connectivity and IoT

元の投稿で解決策を見る

6 返答(返信)
3,679件の閲覧回数
neilporven
Senior Contributor I

Hi Santiago,

Now that I have been able to export the file to a zip file, how do you integrate it to the Kinetis Design Studio?

I tried the import function, but I think I am doing something wrong, the file doesn't appear in the Project Explorer.

Do I have to create a folder in Project Explorer, then import to it?

Thank you.

0 件の賞賛
返信
3,680件の閲覧回数
santiago_lopez
NXP Employee
NXP Employee

Hi Neil,

These are the steps I followed in order to migrate my project.

1. Right click on the mbed project and select Export Program

Step_1.png

2. Click on the drop-down list and select Kinetis Design Studio. Then click on Export

Step_2.png

3. A ZIP file will be downloaded. Extract this file to a known location.

Step_3.png

4. Open Kinetis Design Studio. On the Project Explorer region, right click and select import.

Step_4.png

5. Select Existing Projects into Workspace and click Next

Step_5.png

6. Click on Browse and select the location of the uncompressed folder

Step_6.png

7. Make sure that your project is checked and click on Finish

Step_7.png

After this your project should apear in the Project Explorer

Step_8.png

Saludos

Santiago Lopez -- Connectivity and IoT

3,679件の閲覧回数
neilporven
Senior Contributor I

Gracias Santiago, here's el bravo on Free scale.

0 件の賞賛
返信
3,679件の閲覧回数
santiago_lopez
NXP Employee
NXP Employee

Hi Neil,

There is a tutorial explaining this on the mbed compiler help guide. Go to the compiler and click on the Help icon, then click on the Exporting tab. The last time I checked there was an option for exporting to Kinetis Design Studio.

exporting_project.png

Please let us know if it worked for you.

Saludos

Santiago Lopez -- Connectivity and IoT

0 件の賞賛
返信
3,679件の閲覧回数
neilporven
Senior Contributor I

Hi Santiago,

Disregard the previous message, its not in the help file, but its actually in the export feature.

Saludos,Neil Porven 

0 件の賞賛
返信
3,679件の閲覧回数
neilporven
Senior Contributor I

Hi Santiago,

Unfortunately, I don't see an export feature for the Kinetis Design Studio.  I am very surprised sinceFreescale supports/partners with mbed?  Is there an alternate way of taking the .h and .c files and library includes to the Kinetis Design Studio?

Saludos,Neil Porven

0 件の賞賛
返信