Dependency files for S9KEAZN32AMLH

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dependency files for S9KEAZN32AMLH

2,103件の閲覧回数
Prashant1996
Contributor I

I am trying to use the code generated from MATLAB/Simulink and using the IAR debugger for my motor controls project. I tried finding the hardware dependency files such as GPIO, Pin_mux.h, etc. but was unable to find them in the MCUExpresso config tool. I am using a S9KEAZN32AMLH micro controller with the FRDM-KEAZN32Q64 eval board. All the processors in the list given in the Config tool are MKExxxxxxx format which is unknown for the controller I selected.

Not being familiar with this portion of development, please help me in understanding what files I need for my BLDC motor control application and from where I can download them

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,092件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Could you please provide more details about the files you require? KEA MCUs are not supported by MCUXpresso SDK or MCUXpresso IDE. S32DS is recommended instead.

Best regards,

Felipe

0 件の賞賛
返信

2,078件の閲覧回数
Prashant1996
Contributor I

Hi Felipe,

I tried using the S32DS but could not figure out what I was doing wrong even though I was following the instructions in quick start guide.

Is it possible to schedule a small call so I can share my screen ?

Regards,

Prashant

0 件の賞賛
返信

2,062件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Prashant,

I am sorry but calls are out of the scope of the NXP Technical Communities.

Regards,

Felipe

0 件の賞賛
返信