Dependency files for S9KEAZN32AMLH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dependency files for S9KEAZN32AMLH

2,149 Views
Prashant1996
Contributor I

I am trying to use the code generated from MATLAB/Simulink and using the IAR debugger for my motor controls project. I tried finding the hardware dependency files such as GPIO, Pin_mux.h, etc. but was unable to find them in the MCUExpresso config tool. I am using a S9KEAZN32AMLH micro controller with the FRDM-KEAZN32Q64 eval board. All the processors in the list given in the Config tool are MKExxxxxxx format which is unknown for the controller I selected.

Not being familiar with this portion of development, please help me in understanding what files I need for my BLDC motor control application and from where I can download them

Labels (1)
0 Kudos
Reply
3 Replies

2,138 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Could you please provide more details about the files you require? KEA MCUs are not supported by MCUXpresso SDK or MCUXpresso IDE. S32DS is recommended instead.

Best regards,

Felipe

0 Kudos
Reply

2,124 Views
Prashant1996
Contributor I

Hi Felipe,

I tried using the S32DS but could not figure out what I was doing wrong even though I was following the instructions in quick start guide.

Is it possible to schedule a small call so I can share my screen ?

Regards,

Prashant

0 Kudos
Reply

2,108 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Prashant,

I am sorry but calls are out of the scope of the NXP Technical Communities.

Regards,

Felipe

0 Kudos
Reply