DAC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
5,128 次查看
longjili
Contributor I

hellow,I want use the DAC module of  kea128 to put out the analog signal which will be used as the sensors signal.

The datesheet has been stated:This stepped analog output is also mapped out of the module.But I did not find  the map.

Can anyone tell me where the mapping is?

标记 (1)
0 项奖励
回复
1 解答
4,904 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Longji Li,

   Maybe that description is misleading you.

   Actually, the 6-bit DAC don't have the output pin in the MCU, the content in the reference manual:

This stepped analog output is also mapped out of the module.

  Take care,  it is map out of the module, not the chip. It just means the DAC output have the output from the DAC modue, this output can be used by other module, like CMP.

pastedImage_2.png

   So, this DAC is just used by the CMP, it don't have the output pin in the KEA chip.

Wish it helps you!

Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
4,905 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Longji Li,

   Maybe that description is misleading you.

   Actually, the 6-bit DAC don't have the output pin in the MCU, the content in the reference manual:

This stepped analog output is also mapped out of the module.

  Take care,  it is map out of the module, not the chip. It just means the DAC output have the output from the DAC modue, this output can be used by other module, like CMP.

pastedImage_2.png

   So, this DAC is just used by the CMP, it don't have the output pin in the KEA chip.

Wish it helps you!

Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,904 次查看
longjili
Contributor I

Thank you so much!

0 项奖励
回复
4,904 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

You are welcome.

If your problem is solved, please help me to mark the correct answer, just to close this case.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复