D4D eGUI integration on KINETIS L

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

D4D eGUI integration on KINETIS L

跳至解决方案
1,507 次查看
Etienne
Contributor I

hello

i want to integrate D4D eGUI on Freescale Freedom KL25. I didn't find any straight forward configuration guide for D4D ?

is there anybody had some experience on D4D eGUI on KINETIS or KINETIS L ?

target is to work without MQX

thank you

best regards

Etienne

0 项奖励
回复
1 解答
1,342 次查看
Gargy
NXP Employee
NXP Employee

Hello,

not yet in eGUI core team :-( . But in general it should works with SPI driver without problems.

One think that could make problem is align of data to 4 bytes, because for example BMP decoder is using #pragma(1).

But, in general there should not be issue.

Petr

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,343 次查看
Gargy
NXP Employee
NXP Employee

Hello,

not yet in eGUI core team :-( . But in general it should works with SPI driver without problems.

One think that could make problem is align of data to 4 bytes, because for example BMP decoder is using #pragma(1).

But, in general there should not be issue.

Petr

0 项奖励
回复