D4D eGUI integration on KINETIS L

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

D4D eGUI integration on KINETIS L

Jump to solution
1,580 Views
Etienne
Contributor I

hello

i want to integrate D4D eGUI on Freescale Freedom KL25. I didn't find any straight forward configuration guide for D4D ?

is there anybody had some experience on D4D eGUI on KINETIS or KINETIS L ?

target is to work without MQX

thank you

best regards

Etienne

0 Kudos
Reply
1 Solution
1,415 Views
Gargy
NXP Employee
NXP Employee

Hello,

not yet in eGUI core team :-( . But in general it should works with SPI driver without problems.

One think that could make problem is align of data to 4 bytes, because for example BMP decoder is using #pragma(1).

But, in general there should not be issue.

Petr

View solution in original post

0 Kudos
Reply
1 Reply
1,415 Views
Gargy
NXP Employee
NXP Employee

Hello,

not yet in eGUI core team :-( . But in general it should works with SPI driver without problems.

One think that could make problem is align of data to 4 bytes, because for example BMP decoder is using #pragma(1).

But, in general there should not be issue.

Petr

0 Kudos
Reply