D4D eGUI integration on KINETIS L

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

D4D eGUI integration on KINETIS L

ソリューションへジャンプ
1,492件の閲覧回数
Etienne
Contributor I

hello

i want to integrate D4D eGUI on Freescale Freedom KL25. I didn't find any straight forward configuration guide for D4D ?

is there anybody had some experience on D4D eGUI on KINETIS or KINETIS L ?

target is to work without MQX

thank you

best regards

Etienne

0 件の賞賛
返信
1 解決策
1,327件の閲覧回数
Gargy
NXP Employee
NXP Employee

Hello,

not yet in eGUI core team :-( . But in general it should works with SPI driver without problems.

One think that could make problem is align of data to 4 bytes, because for example BMP decoder is using #pragma(1).

But, in general there should not be issue.

Petr

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,328件の閲覧回数
Gargy
NXP Employee
NXP Employee

Hello,

not yet in eGUI core team :-( . But in general it should works with SPI driver without problems.

One think that could make problem is align of data to 4 bytes, because for example BMP decoder is using #pragma(1).

But, in general there should not be issue.

Petr

0 件の賞賛
返信