Continuous access time interval of K10 FlexBus is too long,WHY?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Continuous access time interval of K10 FlexBus is too long,WHY?

ソリューションへジャンプ
5,047件の閲覧回数
yangzeyong
Contributor III

I use k10 to access sram. port size is 16bit. Data write and read is correct

BUT:  interval time between two access is too Long. so the performace of flexbus is very low

WHY??

Acess SRAM 16 times takes 16us,See the attachment picture

Thanks...

1 解決策
4,892件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check the original code disassembly code.

You can set the compiler optimize level to enhance code execute speed.

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

5 返答(返信)
4,892件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Could you please post the code about write data to external SRAM?


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,892件の閲覧回数
yangzeyong
Contributor III

Hi,Hui_Ma:

     Code is below:

   

#define SRAM_START_ADDRESS   (*(volatile unsigned char*)(0x60000000))
unsigned short LoadWord(unsigned int offset)
{
        return (*(volatile unsigned short*)(&SRAM_START_ADDRESS + offset));
}

void StoreWord(unsigned int offset,unsigned short data)
{
        *(volatile unsigned short*)(&SRAM_START_ADDRESS + offset) = data;
}

void SramWriteBuffer(unsigned short *pBuf,unsigned int addr,unsigned int length)
{
     int s,t;
     if((addr % 2 >0) || (length % 2 >0))
    {
           return;
     }

      s=length/2;
    for(t=0;t<s;t++)
    {
        StoreWord(addr+t*2, *(pBuf+t*2));
    }
 }

///////////////  TestSram : write sram 16 times

void TestSram(void)
{
     unsigned short wbuf[16];
     unsigned int t;
     for(t=0;t<16;t++)
     {
            wbuf[t]=0x1234+t;
      }
     SramWriteBuffer(wbuf,0x0,16*2);
}

Thank you!

0 件の賞賛
返信
4,892件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Could you tried to use below code to do 16 times SRAM write (write to the same address 16 times)? How about the result?

void TestSram(void)
{
     unsigned int t;

     for(t=0;t<16;t++)
     {

         *(volatile unsigned short*)(&SRAM_START_ADDRESS ) = 0x1234;

    }

}

0 件の賞賛
返信
4,892件の閲覧回数
yangzeyong
Contributor III

Hi,Hui_Ma:

    The timing  writing to the same address 16 times looks normal,takes about 4us. Great Job!

    What's the problew of origin code?  Thank you!

p4.PNG

0 件の賞賛
返信
4,893件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check the original code disassembly code.

You can set the compiler optimize level to enhance code execute speed.

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------