Configure Flash Security

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configure Flash Security

840件の閲覧回数
giampietropompo
Contributor I

Hi All,

I'm working with the MK22FN1M0Axxx12, our solution is based on Bootloader + Custom Application.

Now, I should enable the Secure Mode and I'm able to enable it changing the definition of the Flash_Config ( defined into the file startup_*.c ) of the Bootloader.

We have many device in field so I should enable the secure mode by our application, I have done the same steps changing the file startup_*.c of the Application's project but it seems that it doesn't work. 

So I have a doubs, is it possible enabling the secure mode from the application?

Best regards,

Giampietro Pomponio

0 件の賞賛
返信
0 返答(返信)