Code flashing issue in KW45

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code flashing issue in KW45

1,232件の閲覧回数
Chan_17
Contributor III

Hello NxpTeam,

we are  using KW45 and when I received the board BLE was inactive so we activated BLE, and  configured the BLE with Python as mentioned in starter doc. now from that TIME I am not able to Flash the code but was able to use debug , Now even debug also not working. So we are facing issue while flashing code. so please assist on the same.
we followed this process : Getting Started with the KW45B41Z Evaluation Kit | NXP Semiconductors

ラベル(1)
0 件の賞賛
返信
1 返信

1,213件の閲覧回数
sofiaurueta
NXP Employee
NXP Employee

Hello,

Hope you are doing well.

 

Could you be more specific in what process you implemented, what steps of the guide you were able to complete and where you left off?

 

When attempting to flash or debug did you obtain any error logs?

 

Also, could you please clarify what you mean with "activated BLE"? Were you able to program anything on the board before the steps mentioned on the guide?

 

If you have more information you can share with us, it would be greatly appreciated.

 

Best Regards,

Ana Sofia.

0 件の賞賛
返信