Changing microcontroller reference

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Changing microcontroller reference

跳至解决方案
2,026 次查看
guillaumetiffin
Contributor III

Hi all,

I think that my question is a newbie question but this problem can block my project.

I'm using CW 10.4, MQX 4.0 and MK60FX512VLQ15 microcontroller.

To start the project I used the tower k60f120m.

I would like to do the migration to the new device.

It's a custom board and I use the MQX BSP cloning wizard in order to use the new board.

Between the MK60F1NM0 and the MK60FX512VLQ15, there are some difference in mapping the program addresses and so on.

How can I do the migration easily between those two microcontroller?

What are the file that I need to change and where can I find them?

The project seems to run on my custom board without changing mapping but when I will do the bootloader I think that I will have some troubles.

I don't use processor expert to generate code.

Please help me.

Thank you for your help.

Best regards,

Guillaume

0 项奖励
回复
1 解答
1,773 次查看
hectorsanchez
Contributor IV

Hi Guillaume,

I recommend you to check this thread:

How to migrate between two different K40 chips?

Hope this helps, keep me informed if this solved your problem.

Best regards,

Hector Sanchez

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,773 次查看
guillaumetiffin
Contributor III

Hi Hector,

It works for me.

I thought that it will be more difficult but no.

Thank you very much !!

Regards,

Guillaume

0 项奖励
回复
1,774 次查看
hectorsanchez
Contributor IV

Hi Guillaume,

I recommend you to check this thread:

How to migrate between two different K40 chips?

Hope this helps, keep me informed if this solved your problem.

Best regards,

Hector Sanchez

0 项奖励
回复