Changing microcontroller reference

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing microcontroller reference

ソリューションへジャンプ
2,119件の閲覧回数
guillaumetiffin
Contributor III

Hi all,

I think that my question is a newbie question but this problem can block my project.

I'm using CW 10.4, MQX 4.0 and MK60FX512VLQ15 microcontroller.

To start the project I used the tower k60f120m.

I would like to do the migration to the new device.

It's a custom board and I use the MQX BSP cloning wizard in order to use the new board.

Between the MK60F1NM0 and the MK60FX512VLQ15, there are some difference in mapping the program addresses and so on.

How can I do the migration easily between those two microcontroller?

What are the file that I need to change and where can I find them?

The project seems to run on my custom board without changing mapping but when I will do the bootloader I think that I will have some troubles.

I don't use processor expert to generate code.

Please help me.

Thank you for your help.

Best regards,

Guillaume

0 件の賞賛
返信
1 解決策
1,866件の閲覧回数
hectorsanchez
Contributor IV

Hi Guillaume,

I recommend you to check this thread:

How to migrate between two different K40 chips?

Hope this helps, keep me informed if this solved your problem.

Best regards,

Hector Sanchez

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,866件の閲覧回数
guillaumetiffin
Contributor III

Hi Hector,

It works for me.

I thought that it will be more difficult but no.

Thank you very much !!

Regards,

Guillaume

0 件の賞賛
返信
1,866件の閲覧回数
hectorsanchez
Contributor IV

Hi Guillaume,

I recommend you to check this thread:

How to migrate between two different K40 chips?

Hope this helps, keep me informed if this solved your problem.

Best regards,

Hector Sanchez

0 件の賞賛
返信