Can not import K60N512 project.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can not import K60N512 project.

跳至解决方案
1,430 次查看
danielchai
Senior Contributor I

Hi All,

I just installed the MQX3.8.1 patch for GS1500M. When I follow the instruction to import the project httpsrv_twrk60n512 from  rtcs\examples\gstwr_httpsrv. It gives me error:


Error processing changed links in project description file.

Details:

No file system is defined for scheme:

Any ideas about this?

Thanks.

标记 (4)
1 解答
1,240 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

in addition,  please also check properties setting "Resource", "Linked Resources", "Path Variables" check if the path setting is consistent with the project/system path. then go to project properties setting, "C/C++ General", "Paths and Symbols", check if the path is right.

在原帖中查看解决方案

3 回复数
1,241 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

in addition,  please also check properties setting "Resource", "Linked Resources", "Path Variables" check if the path setting is consistent with the project/system path. then go to project properties setting, "C/C++ General", "Paths and Symbols", check if the path is right.

1,240 次查看
Monica
Senior Contributor III

Hello Daniel,

did this help to move on with your project?

Please don't forget to keep us posted! :smileywink:

Best regards,

Monica

0 项奖励
回复
1,240 次查看
apanecatl
Senior Contributor II

I think you might have installed the MQX 3.8 patch in the wrong directory, you need to install it in the following path:

C:\Freescale\MQX3.8 instead of using the default path C:\Program files\Freescale\MQX3.8

0 项奖励
回复