Can not import K60N512 project.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can not import K60N512 project.

ソリューションへジャンプ
2,191件の閲覧回数
danielchai
Senior Contributor I

Hi All,

I just installed the MQX3.8.1 patch for GS1500M. When I follow the instruction to import the project httpsrv_twrk60n512 from  rtcs\examples\gstwr_httpsrv. It gives me error:


Error processing changed links in project description file.

Details:

No file system is defined for scheme:

Any ideas about this?

Thanks.

1 解決策
2,001件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

in addition,  please also check properties setting "Resource", "Linked Resources", "Path Variables" check if the path setting is consistent with the project/system path. then go to project properties setting, "C/C++ General", "Paths and Symbols", check if the path is right.

元の投稿で解決策を見る

3 返答(返信)
2,002件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

in addition,  please also check properties setting "Resource", "Linked Resources", "Path Variables" check if the path setting is consistent with the project/system path. then go to project properties setting, "C/C++ General", "Paths and Symbols", check if the path is right.

2,001件の閲覧回数
Monica
Senior Contributor III

Hello Daniel,

did this help to move on with your project?

Please don't forget to keep us posted! :smileywink:

Best regards,

Monica

0 件の賞賛
返信
2,001件の閲覧回数
apanecatl
Senior Contributor II

I think you might have installed the MQX 3.8 patch in the wrong directory, you need to install it in the following path:

C:\Freescale\MQX3.8 instead of using the default path C:\Program files\Freescale\MQX3.8

0 件の賞賛
返信