Can not import K60N512 project.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not import K60N512 project.

Jump to solution
2,142 Views
danielchai
Senior Contributor I

Hi All,

I just installed the MQX3.8.1 patch for GS1500M. When I follow the instruction to import the project httpsrv_twrk60n512 from  rtcs\examples\gstwr_httpsrv. It gives me error:


Error processing changed links in project description file.

Details:

No file system is defined for scheme:

Any ideas about this?

Thanks.

1 Solution
1,952 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

in addition,  please also check properties setting "Resource", "Linked Resources", "Path Variables" check if the path setting is consistent with the project/system path. then go to project properties setting, "C/C++ General", "Paths and Symbols", check if the path is right.

View solution in original post

3 Replies
1,953 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

in addition,  please also check properties setting "Resource", "Linked Resources", "Path Variables" check if the path setting is consistent with the project/system path. then go to project properties setting, "C/C++ General", "Paths and Symbols", check if the path is right.

1,952 Views
Monica
Senior Contributor III

Hello Daniel,

did this help to move on with your project?

Please don't forget to keep us posted! :smileywink:

Best regards,

Monica

0 Kudos
Reply
1,952 Views
apanecatl
Senior Contributor II

I think you might have installed the MQX 3.8 patch in the wrong directory, you need to install it in the following path:

C:\Freescale\MQX3.8 instead of using the default path C:\Program files\Freescale\MQX3.8

0 Kudos
Reply