Can K21 USBDCD use for detect VBUS status?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can K21 USBDCD use for detect VBUS status?

跳至解决方案
1,024 次查看
jimyang
Contributor II

Hi,

Anybody tell me if K21 USBDCD can use for detect VBUS status? And how to do?

Thanks!

Jim

标签 (1)
0 项奖励
回复
1 解答
901 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Jim Yang

We recommend to use a GPIO pin as VBUS detection, which also could wake up the chip from all low power mode (includes LLS mode or VLLSx mode (using LLWU module with external pin)).

 

The VBUS connects to VREGIN and a GPIO pin doesn't cause conflict. I think customer can fly a wise to connect VBUS with related GPIO pin.


Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
902 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Jim Yang

We recommend to use a GPIO pin as VBUS detection, which also could wake up the chip from all low power mode (includes LLS mode or VLLSx mode (using LLWU module with external pin)).

 

The VBUS connects to VREGIN and a GPIO pin doesn't cause conflict. I think customer can fly a wise to connect VBUS with related GPIO pin.


Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复