Can K21 USBDCD use for detect VBUS status?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can K21 USBDCD use for detect VBUS status?

ソリューションへジャンプ
1,030件の閲覧回数
jimyang
Contributor II

Hi,

Anybody tell me if K21 USBDCD can use for detect VBUS status? And how to do?

Thanks!

Jim

ラベル(1)
0 件の賞賛
返信
1 解決策
907件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Jim Yang

We recommend to use a GPIO pin as VBUS detection, which also could wake up the chip from all low power mode (includes LLS mode or VLLSx mode (using LLWU module with external pin)).

 

The VBUS connects to VREGIN and a GPIO pin doesn't cause conflict. I think customer can fly a wise to connect VBUS with related GPIO pin.


Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
908件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Jim Yang

We recommend to use a GPIO pin as VBUS detection, which also could wake up the chip from all low power mode (includes LLS mode or VLLSx mode (using LLWU module with external pin)).

 

The VBUS connects to VREGIN and a GPIO pin doesn't cause conflict. I think customer can fly a wise to connect VBUS with related GPIO pin.


Hope this information helps you
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信