CW10.5 debug issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW10.5 debug issue

2,123件の閲覧回数
kevinmc
Contributor II

Hi,

I'm running a project succesfully in CW10.3, now I've updated to 10.5 and I get the following problem when trying to debug via ' download':

INF:CRC-16 Error in block. (File = $892C, Device = $2DD1)

It appears to compile and download without issue, however it falls over on checking?

We can debug using 'attach'.

What has changed here in CW10.5?? I would really like to use 'Download' debug method.

Cheers,

KMC

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,909件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Kevin:

Could you provide more details? What is the specific error you see?

If possible please share a screenshot of the issue. Also it is always good to try with a new bareboard project to determine if the problem is with CodeWarrior <-> debugger tool or specifc to your project.


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,909件の閲覧回数
Robinwithu
Senior Contributor I

Hi Kevin,

can you mail me your project (Code) i can compile here , having CW 10.5  and PE USB Multilink Interface programming Hardware.

Thanks and Regards,

Robin

0 件の賞賛
返信

1,909件の閲覧回数
Robinwithu
Senior Contributor I

Hi Kevin,

May be this is useful for you ,please go through it.

CW10.5 debug problem &gt; Cannot enter background mode. Check connections.

Thanks and Regards,

Robin

0 件の賞賛
返信