CW10.5 debug issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW10.5 debug issue

2,223 次查看
kevinmc
Junior Contributor II

Hi,

I'm running a project succesfully in CW10.3, now I've updated to 10.5 and I get the following problem when trying to debug via ' download':

INF:CRC-16 Error in block. (File = $892C, Device = $2DD1)

It appears to compile and download without issue, however it falls over on checking?

We can debug using 'attach'.

What has changed here in CW10.5?? I would really like to use 'Download' debug method.

Cheers,

KMC

标签 (1)
0 项奖励
回复
3 回复数

2,009 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Kevin:

Could you provide more details? What is the specific error you see?

If possible please share a screenshot of the issue. Also it is always good to try with a new bareboard project to determine if the problem is with CodeWarrior <-> debugger tool or specifc to your project.


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,009 次查看
Robinwithu
Senior Contributor I

Hi Kevin,

can you mail me your project (Code) i can compile here , having CW 10.5  and PE USB Multilink Interface programming Hardware.

Thanks and Regards,

Robin

0 项奖励
回复

2,009 次查看
Robinwithu
Senior Contributor I

Hi Kevin,

May be this is useful for you ,please go through it.

CW10.5 debug problem &gt; Cannot enter background mode. Check connections.

Thanks and Regards,

Robin

0 项奖励
回复