VREFH and VREFL connections for K60 when not using ADC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

VREFH and VREFL connections for K60 when not using ADC

1,405 次查看
tommyb
Contributor I

I am trying to determine if I can tie my VREFH and VREFL lines directly to digital ground if I am not using the ADC of the K60.  I of course would keep VDDA connected to VDD, and put a decoupling cap on VREF_OUT, but wondering if I need to decouple VREFH and VREFL if I am not using them.

0 项奖励
回复
1 回复

1,140 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Tommy:

The recommendation is to connect VREFH to VDD and VREFL to GND. This helps with the noise immunity.


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复